2008-01-24 11:24 PM
STR751 ADC and Power Supply Question
2008-01-24 10:05 PM
I need some help to understand the datasheet of the STR751 ARM, because some sentences are very unclear:
There is said that the VDDA_ADC and VSSA_ADC pins are the analog power supply of the A/D converter cell, but how can I set the reference-Voltage? I need 0-5V Measurement. There is a chapter named ''Power supply schemes'' but there is nothing said about the STR751-µC -> Does it work with 5V? Can I set VDDA_ADC higher than VDD_IO? Why is USB disabled in 5V-Mode?2008-01-24 11:24 PM
Reference manual says that VDDA_ADC must be equal to VDD_IO. Since it is ''sensitive'' supply, you can use better filtering for this pin. That's all...
I'm in doubt whether you will find any answer for your second question - Why is USB disable in 5V mode...