2006-09-19 10:52 PM
2006-09-19 10:12 PM
Hi,
in the data sheet pin P1.15 of the STR710 is marked as an interrupt input. In the reference P1.15 is not listed in the XTI list. :-o So i wonder if and how I can use P1.15 as interrupt input. Maybe there is a trick with the HDLC module? Regards, Joerg2006-09-19 10:37 PM
In my
http://www.st.com/stonline/books/pdf/docs/10350.pdf#search=''STR71x'';
P1.15 is not marked as interrupt input at all... So no wonder that it is not in the XTI list.2006-09-19 10:52 PM
:-(
Yes they changed it: '22-May-2006: removed x in interrupt column for P1.15 and P1.12 in Table 3 and Table 6' I got the datasheet from oktober 2005! That sucks! Thanks anyway....