cancel
Showing results for 
Search instead for 
Did you mean: 

STR710-Eval UART problem

mehanathan
Associate
Posted on August 15, 2007 at 09:01

STR710-Eval UART problem

2 REPLIES 2
mehanathan
Associate
Posted on July 06, 2007 at 13:49

Hello everyone. I am using a STR710-Eval board, and am trying to run the UART interrupt sample code that comes with RIDE.

My problem is that I obtain different characters in hyperterminal from what I transmit. I have not modified any of the settings in the default code (Baud rate 9600, 8 bit data with no parity, 1 stop bit). I have also set hyperterminal up to match the above configuration.

I hope someone here has an idea of what is going on, as I've spent most of today trying to figure out how to get the correct characters appearing. Thanks in advance.

mehdi239955
Associate II
Posted on August 15, 2007 at 09:01

Hi Mehanathan,

Are you speaking about the ST lib example which comes with RIDE?(.\RIDE\EXAMPLES\STRX\STR71XLIB\UART\INTERRUPT)

I've tested it and nothing is wrong ! i've got the message on the terminal.

Could check if the jumpers on Reva board are set (Rx and Tx jumpers)?

Quote:

I have also set hyperterminal up to match the above configuration.

Please also check that in the hyperterminal configuration the flow control = None.

Regards,

MBS