cancel
Showing results for 
Search instead for 
Did you mean: 

STR7 packet buffer USB limitation

francesco23
Associate II
Posted on October 30, 2008 at 10:34

STR7 packet buffer USB limitation

11 REPLIES 11
anis23
Associate II
Posted on May 12, 2006 at 11:27

Hi Bassof,

I mean by reset interrupt the interruption occurred just after an USB reset (when you plug the USB cable). For a complete example you can see the USB software library provide by ST in the internet web site (for the USB reset you can se the file ''usb_prop.c'' function ''MOUSE_Reset()'': this function is called after each USB reset).

You are welcome.

Regards,

AnisAS

😉

francesco23
Associate II
Posted on May 12, 2006 at 12:23

Hi AnisAs,

Thanks for all, :-]

a bientôt,

Bassof