cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H407ve FSMC with SRAM

BEKABEN
Associate II

Hi,

I'm trying to set up STM32F407Ve (ST Blackboard) FSMC with SRAM 16 bits of data and 10 bits of address on STM32CUBEIDE. However, all I get on the list :

LCD Interface, Muxed NOR flash, and MUXE PSRAM.

How can I enable SRAM ?

 

1 REPLY 1
TDK
Guru

The LQFP100 package is missing pins which are necessary for driving SRAM. Because of that, SRAM isn't presented as an available FSMC option for this chip in CubeMX.

There's a note in the datasheet which says this, but it's easy to miss.

TDK_0-1691515445554.png

 

If you feel a post has answered your question, please click "Accept as Solution".