cancel
Showing results for 
Search instead for 
Did you mean: 

STHV800 single polarity HV

serghei
Associate II
Posted on February 18, 2016 at 10:16

Can I use only one HV power source (HVM or HVP)? I need pulses single polarity.

#sthv800-single-polarity-hv
1 REPLY 1
ricciardo.antonio
Associate II
Posted on March 03, 2016 at 09:47

Hello Serghei,

Yes, you can, for instance if you need only HVP, the suggestion is to connect anyway the negative voltage supplies, namely:

- HVM=HVM_CW= 0V (or -3V)

- VDDM= -3V (mandatory)

If you have to use only HVM, do connect anyway HVP=HVP_CW=0V (or +3V) and VDDP= +3V (mandatory)

Please, for further support contact directly ST prod. team in division thru my person:

mailto:antonio.ricciardo@st.com

, so in this way we can share additional details about your prj

Regards

Antonio