2006-06-28 09:27 PM
2006-06-06 10:09 PM
Does anyone know how to get the st10flasher.lib to the st10flasher.dll of the 2.4B flasher tool? Even our Distributor seems unable to get it.
It is needed to recompile our command line 'frontend' to the DLL. For the old Flasher there was a 'DevelopmentKit' with examples and the linker library: Verzeichnis von E:\Programme\STM\ST10Flasher\DevelopmentKit 06.12.2005 15:09 <DIR> . 06.12.2005 15:09 <DIR> .. 31.05.2001 15:03 6.472 basicinterface.h 06.12.2005 15:09 <DIR> CPP_Sample 31.05.2001 15:02 4.621 Dll_interface.bas 31.05.2001 15:03 75.170 st10flasher.exp 31.05.2001 15:03 126.516 st10flasher.lib <- linker lib 4 Datei(en) 212.779 Bytes Verzeichnis von E:\Programme\STM\ST10Flasher\DevelopmentKit\CPP_Sample 06.12.2005 15:09 <DIR> . 06.12.2005 15:09 <DIR> .. 31.05.2001 15:03 1.206 ReadMe.txt 31.05.2001 15:03 3.075 Samples.cpp 31.05.2001 15:03 4.643 Samples.dsp 31.05.2001 15:03 621 Samples.dsw 31.05.2001 15:03 295 StdAfx.cpp 31.05.2001 15:03 707 StdAfx.h 6 Datei(en) 10.547 Bytes Is there an update to this, too? Thank you..2006-06-08 01:44 AM
Does somebody have documentation on the flasher DLL? Or code examples how to call it directly from 'C' without the linker lib?
Thank you.2006-06-28 09:27 PM
2010-03-31 01:31 PM