2003-06-15 11:42 PM
2003-06-13 03:18 AM
I intend to use the ST-REALIZER II for ST72264 program development.
Can I use the InDART STX/D to transfer the ST-REALIZER made target hexcode to the target? Looking forward to your answer....2003-06-15 09:46 PM
Hi,
In the project folder you will find a .S19 file Using the inDART, select the programmer and device Select File > Load > Code Buffer change the format to Motorola S-record and locate the above file. Ensure you also configure the option bytes regards, Simon Anglia2003-06-15 11:42 PM
Thank you!