cancel
Showing results for 
Search instead for 
Did you mean: 

ST M24C02-FMC6TG

TPak.1
Associate

I need a formal MTBF/FIT/Reliability report for the subject PN for my product life prediction. Thanks.

I need to see the FIT's at different confident levels, temperatures, ..etc. Is there a site link I can obtain the data similar your competitors offer.

1 REPLY 1
Pierre P.
Senior III

Hello,

Find below the Fit values for this M24C02-FMC6TG:

@25°C:

0.1 - 60% Confidence level

0.3 - 90% Confidence level

@55°C:

1.5 - 60% Confidence level

3.8 - 90% Confidence level

@85°C:

12.2 - 60% Confidence level

30.6 - 90% Confidence level

BR

Team EEPROM suPPort