2008-08-22 04:08 AM
2011-05-17 12:55 AM
Hi there
I tried to pass around this, reworking the functions of 91x_SSP, to work directly with registries, and this is working, except one register, the DR register, each time i try to write to it, it fills the bytes up with 0xFF! does any one know how to write to it? Thankx :-o2011-05-17 12:55 AM
The DR register is tied to the transmit & receive FIFOs for the SSP. When you write to it, it loads the word into the transmit buffer. But when you read from it, it reads the next entry in the receive buffer. So you shouldn't expect to see the same value you just wrote to it when you read it.
matt2011-05-17 12:55 AM
hi matt!
Thanks again for the tip, but i've tried other prespective, and i've compiled and runned ST SSP example, once more the problem is the same!!! The doomed processor goes on looping in here and stay in there forever!!! code part: ... /* Master to slave transfer procedure */ while(Tx_Idx { SSP_SendData(SSP0, SSP0_Buffer_Tx[Tx_Idx++]); :-Z while(SSP_GetFlagStatus(SSP1, SSP_FLAG_RxFifoNotEmpty)==RESET); SSP1_Buffer_Rx[Rx_Idx++] = SSP_ReceiveData(SSP1); } ... in this while loop. Thanks again2011-05-17 12:55 AM
Have you checked your HW connections?
SSP0 MOSI -> SSP1 MOSI SSP0 MISO -> SSP0 MISO SSPO NSS -> pull high SSP1 NSS -> pull low