2008-09-04 11:39 PM
2011-05-17 12:55 AM
Hello ricardo.marinheiro,
Did you measure the IDD(1.8V) and IDDQ(3.3V) in your board? It can be a hardware problem. Or try to erase the flash and try to load the program again. Please do these tests and let me know. Best regards, mirou.2011-05-17 12:55 AM
hi everyone
I'm complitely blocked in here... i can´t do anything!!! Fri Aug 22 13:41:50 2008: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 5.0 Kickstart\ARM\config\flashloader\ST\FlashSTR91x.mac Fri Aug 22 13:41:50 2008: DLL version: V3.90b, compiled Aug 21 2008 14:51:23 Fri Aug 22 13:41:50 2008: Firmware: J-Link compiled Jul 30 2008 11:24:37 ARM Rev.5 Fri Aug 22 13:41:50 2008: JTAG speed is using adaptive clocking (RTCK signal) Fri Aug 22 13:41:50 2008: Initial reset was performed Fri Aug 22 13:41:50 2008: TotalIRLen = ?, IRPrint = 0x..00000000000000000000000000000000 Fri Aug 22 13:41:52 2008: Fatal error: Invalid core Id. (0) have you ever seen this?... can anyone help with this?? thank you :-[2011-05-17 12:55 AM
Hi
The problem was BootLoader became all messed up and i just used a SEEGER tool to upload it again to his place, and all went well. By saying that BootLoader was a mess, it was what i assumed once the j-Link couldn't sync with ARM becouse it was no RTC clock to do it. Hope it help =)