2004-01-27 03:01 AM
2004-01-17 07:26 AM
If own an old ST6 Starter-Kit with a programmer called ''ST62E1X Basic Programmer''. Unfortunatly discs included are 5 1/4
The Windows Eprommer software available does not list this board. Is there a Windows (2000/XP) version, that supports this bord? If not, where can I get the originl programmer software (I guess DOS)? [ This message was edited by: Yavuz on 17-01-2004 20:57 ]2004-01-27 03:01 AM
The board which you are trying to use is very very old board and is not supported now. Windows Eprommer (Winee) also does not support this board. That is why it is not in the list. Also this board may not work well with the high speed PCs.
I will suggest you to use the new starter kit which is a low cost board and able to perform many functions. It can be used as a programmer and application board etc.