2006-08-27 10:41 PM
2006-08-25 04:57 AM
Hi,
Is it possible to transmit informaion on SCI ports with a bauds rate equals to 57600 or not? I have ST72334 with a quartz (8MHz).It doesn't work. But with a quarz 16MHz, is it possible to communicate? SCIETPR=0x09; => 55 555 bauds So, the mistake is 3.5%. Is it good or not ? thank you. [ This message was edited by: Philippe13 on 25-08-2006 17:41 ]2006-08-27 10:41 PM
Hi Philippe,
with standard transmitter it should work. Although I didn't find anything about the required accuracy I remember an allowed tolerance of 5%. But also consider the maximum cable-length. From my experience it should not exceed 1.5m with a baud-rate of 57,6kbauds. By the way: I prefer to use a crystal of 7.3728MHz or even 3.6864MHz wich both are usual standards. You can reach baud-rates up to 115.2kbps with the 3,6864MHz crystal. The only little inconvenience resulting from this solution: You must calculate all the timings depending on this frequency. Best regards WoRo