cancel
Showing results for 
Search instead for 
Did you mean: 

Routing for USBLC6-2SC6

w_I
Associate

Hi,

I am creating my own PCB based on the Nucleo144pin board. From what I understand, the USBLC6-2SC6 is meant to be an ESD protection IC. The USBLC6-2 datasheet recommends that the input is not connected to the output. However, the inputs from the USB connector is shorted to the output of the USBLC6-2SC6 in the Nucleo144pin board. Is there an intended function for this or is it an error?

75a81f4f-f72b-4335-8098-f16a96d3363e.jpg53e3ca53-5fab-4347-b044-2142647b0fc9.jpgPCB.JPG

0 REPLIES 0