2009-01-29 11:51 PM
2009-01-23 04:45 AM
Hi,
There are 2 bytes of E2 allocated for storing user osc calibration information, RCCRL_USER and RCCRH_USER. Q1: Do ST program these locations with the RCCR factory calibration values in production, or are these left blank? Q2: If the device is protected then unprotected, are these values erased? Thanks, Martin.2009-01-28 12:41 AM
Hello Martin,
Q1: The RCCRH_USER are not factory programmed by ST. They are left blank. Q2: If the device is protected then unprotected (ROP set then removed), those values are erased. Best regards, Seb2009-01-29 11:51 PM
Hi Seb,
Thanks for confirming. Martin.