Posted on May 17, 2011 at 15:02Hello l.yeganeh, The maximum frequency available for the I2C peripheral on STM8S is 24MHz. It can not be more as it is the maximum input frequency of the MCU. Best regards, Seb
Posted on May 17, 2011 at 15:02Hello l.yeganeh, The option bytes are in fact located at the end of EEPROM memory area at adress 0x4800. It's here that the option bytes are programed by the tools (STVP or STVD). So to read option bytes you just have ...
Posted on May 17, 2011 at 12:37Hello h.s.low, Here it is the forum for ST7 8 bit micro. For STM32 questions, please post your message in the appropriate forum called ARM Cortex-M3 STM32 (http://www.st.com/mcu/forumsid-23.html). Thank you for your un...
Posted on January 28, 2009 at 09:41Hello Martin, Q1: The RCCRH_USER are not factory programmed by ST. They are left blank. Q2: If the device is protected then unprotected (ROP set then removed), those values are erased. Best regards, Seb
Posted on June 16, 2008 at 10:25Hello cicciounico, In ST7 lite there are two ways of using the watchdog. - Watchdog hardware: In this configuration the watchdog will start to count immediately after the micro startup. Before entering in your endless...