2004-08-04 09:25 AM
2011-05-17 03:02 AM
Hi,
I’m having some problems with my project somebody can help me? My memory map is: Main Flash: FS0 – PAG: 0 – 0X0000 ~ 0X3FFF FS1 – PAG: 0 – 0X4000 ~ 0X7FFF FS2 – PAG: 0 – 0X8000 ~ 0XBFFF FS3 – PAG: 0 – 0XC000 ~ 0XFFFF Others: RS0 – 0XC000 ~ 0XDFF CSIOP – 0XE00 ~ 0XE0FF LCD_E – 0XE100 ~ 0XE1FF Secondary flash: CSBOOT0 – 0X0000 ~ 0X1FFF CSBOOT1 – 0X2000 ~ 0X3FFF CSBOOT2 – 0X4000 ~ 0X5FFF CSBOOT3 – 0X6000 ~ 0X7FFF Main Flash: Data Space Only Secondary Flash: Program Space Only I’m running my IAP application at CSBOOT flash, but I can’t make my LCD routines works. If I put this same program at the main flash it works fine. Can it happen because my LCD_E logic is mapped in the same address of main flash? How can I resolve this? Thanks in advance Sombra