cancel
Showing results for 
Search instead for 
Did you mean: 

re program failed since after first 2 to 3 times programming OK!

hg-chen
Associate II
Posted on September 10, 2004 at 06:00

re program failed since after first 2 to 3 times programming OK!

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
hg-chen
Associate II
Posted on May 17, 2011 at 12:02

uPSD3234BV-24U6 is used.

at first 2 to 3 times, programing is OK, but since then,

re program failed!

any suggestion?
joseph2399
Associate II
Posted on May 17, 2011 at 12:02

Verify that the FlashLink device and JTAG connection to the DK3200 is good by running the FlashLink Connect Test and the Target Connect Test (these tests are found in the H/W setup located in the JTAP-ISP Operations Window). Be sure to do an erase all in case the security bits were set. Check your power supplies to the device.

hg-chen
Associate II
Posted on May 17, 2011 at 12:02

Error message as below: also attachement

Erse Full chip----Fail

Fail to erase full chip

Program operation unsuccesul----
hg-chen
Associate II
Posted on May 17, 2011 at 12:02

error message as attachement

hg-chen
Associate II
Posted on May 17, 2011 at 12:02

the loop test result as attachement!

any idea?