2005-12-11 10:04 PM
2011-05-17 03:08 AM
Hello!
I am very new to the upsd33xx and I am at the moment trying out the funcionalities of the PLD. To give any logical level to Port B from the MCU as a GPIO is no problem, but to receive a value from a Port pin as GPIO does not work. But it might be, that i make some mistake in memory addressing. Here is my configuration: .abl-file: jtagsel = !_reset; rs0 = ((address >= ^h0000) & (address <= ^h1FFF)); csiop = ((address >= ^h2000) & (address <= ^h20FF)); fs0 = ((address >= ^h0000) & (address <= ^h7FFF)); fs1 = ((page == 0) & (address >= ^h8000) & (address <= ^hFFFF)); fs2 = ((page == 1) & (address >= ^h8000) & (address <= ^hFFFF)); fs3 = ((page == 2) & (address >= ^h8000) & (address <= ^hFFFF)); fs4 = ((page == 3) & (address >= ^h8000) & (address <= ^hFFFF)); fs5 = ((page == 4) & (address >= ^h8000) & (address <= ^hFFFF)); fs6 = ((page == 5) & (address >= ^h8000) & (address <= ^hFFFF)); fs7 = ((page == 6) & (address >= ^h8000) & (address <= ^hFFFF)); csboot0 = ((address >= ^h8000) & (address <= ^h9FFF)); csboot1 = ((address >= ^hA000) & (address <= ^hBFFF)); csboot2 = ((address >= ^hC000) & (address <= ^hDFFF)); csboot3 = ((address >= ^hE000) & (address <= ^hFFFF)); Code for configuration and data transfers: ;configuration of the direction of Port B GPIO MOV A,#00011111b MOV DPTR,#DIRECTION_B MOVX @DPTR,A ;OUTPUT ENABLE for the output pins MOV A,#00011111b MOV DPTR,#OUTENABLE_B MOVX @DPTR,A ;send data to PORT B MOV A,#00011111b MOV DPTR,#DATAOUT_B MOVX @DPTR,A receive data from Port B MOV DPTR,#DATAIN_B MOVX A,@DPTR PSD_REGISTER_CONFIGURATION: DATAIN_A data 2000H; // PSD_REG_BASE +0x00 DATAIN_B data 2001H; // +0x01 CONTROL_A data 2002H; // +0x02 CONTROL_B data 2003H; // +0x03 DATAOUT_A data 2004H; // +0x04 DATAOUT_B data 2005H; // +0x05 DIRECTION_A data 2006H; // +0x06 DIRECTION_B data 2007H; // +0x07 DRIVE_A data 2008H; // +0x08 DRIVE_B data 2009H; // +0x09 IMC_A data 200AH; // +0x0A IMC_B data 200BH; // +0x0B OUTENABLE_A data 200CH; // +0x0C OUTENABLE_B data 200DH; // +0x0D Thanks for your help! kind regards harryplotter42011-05-17 03:08 AM
Hello!
I'm sorry for not answering for such a long time. but, i also fixed the problem. It was just some configuration missmatch between the MCU memory description and the PSD memory description. Thanks!