cancel
Showing results for 
Search instead for 
Did you mean: 

Parrallel Processing in st10F269

abdulhameed6
Associate II
Posted on June 01, 2006 at 14:47

Parrallel Processing in st10F269

2 REPLIES 2
abdulhameed6
Associate II
Posted on May 25, 2006 at 10:54

dear

i am using st10F269 and using c as programming language and keil compiler for compilation.

i am receiving serial data at 9600 bps. after processing on the received data, i am trasmitting that data at 9600.

1. my first question is that is it possible that i can have parrallel processing i.e that reception and Transmission routine are executing in parrallel with the normal processing of data.

one suggestted thing can be that

:-0 i want that i define a array in which data is received and after some time i check it and again keep busy in doing processing. in the same way i put my transmission data in a array and processor transmit that data in parrallel when give signal to it in parrallel with normal processing of data.

2. my Second question is that can i have different baud rate and parity settings for serial port Transmission & Reception available in st10f269.

what is the role of Peripheral Event controller.

kindly provide some code examples if the above things are possible with st10f269.

best regards.

Hello.

[ This message was edited by: Hello on 26-05-2006 05:54 ]

[ This message was edited by: Hello on 31-05-2006 06:29 ]

abdulhameed6
Associate II
Posted on June 01, 2006 at 14:47

dear

how can i stop the program counter not to go to serial reception or transmission routine when some data transmitted or received and i have interrupt based routine.

Best regards.

Hello

[ This message was edited by: Hello on 02-06-2006 17:38 ]