Posted on June 01, 2006 at 14:47dear how can i stop the program counter not to go to serial reception or transmission routine when some data transmitted or received and i have interrupt based routine. Best regards. Hello [ This message was edited b...
Posted on May 25, 2006 at 10:54dear i am using st10F269 and using c as programming language and keil compiler for compilation. i am receiving serial data at 9600 bps. after processing on the received data, i am trasmitting that data at 9600. 1. my ...
Posted on May 11, 2006 at 10:13Dear i kept check the option in target enable xram1 and xram2.now i will also keep enable these values in startup file and will check the result. is these option should be same/necessory to set both in keil ide and sta...
Posted on May 10, 2006 at 11:10dear uiSerialTx located in Ndata0 at address of 0x0F616 according to new map file in which program is running Best regards Hello