cancel
Showing results for 
Search instead for 
Did you mean: 

Oscillator Start up time

giovanni239955
Associate II
Posted on September 02, 2003 at 15:03

Oscillator Start up time

2 REPLIES 2
giovanni239955
Associate II
Posted on May 17, 2011 at 11:34

I notice that, using a ST92F150, with a 4 MHz crystal, when I exit from Stop Mode the first instruction is executed after about 10 ms. This is not the same thing declared in the datasheet (max 5 ms).

Can you help me to fasten this behaviour? I need to be fast in order to acknowledge a message received from CAN bus.

Many thanks.

kapil
Associate II
Posted on May 17, 2011 at 11:34

This problem may arise due to the fact that after exiting the stop mode the internal clock frequency is reduced to 2 Mhz