2006-02-15 10:12 PM
MMC or SD card in SPI mode with STR710
2006-02-14 08:29 PM
Hello everybody.
Can I transfer data on a MMC or SD memory card (in SPI mode) with the BSPI interface of STR710 micro-controller? Thank you2006-02-14 09:29 PM
Yes, it is possible.
2006-02-15 01:15 AM
Thank you for your answer.
Did you already use SPI signals for reading and writing on a SD card? Is there a free example on the Web for the memory card driver?2006-02-15 10:12 PM
Look at
best regards, Frank Andersen