2005-01-08 04:34 AM
2011-05-17 03:05 AM
Hello,
I use the uPSD3234a. I have a problem with the page memory configuration. I used to have all my code on the boot flash. and use page 0 and 1 for data. now since my code got larger, I set page 0 and 1 to contain some of my code. The program runs good. however the method I used before for writing parameter to a page doesn't work any more. I think it is because now both flashs are set to ''Program Space Only'' (the pogram does not run in any other way) in the PSDsoft Express. here is how I used it before: here are the access addreses codes: PSD8xx_reg.PAGE = 0x02;// flash sector 0 selected FLASH_COM_X555 = (uchar xdata *)(FLASH_PARAM_ADDR + 0x0555); FLASH_COM_XAAA = (uchar xdata *)(FLASH_PARAM_ADDR + 0x0AAA); FLASH_COM_X000 = (uchar xdata *)(FLASH_PARAM_ADDR); then for example erase sector code *(FLASH_COM_X555) = 0xAA; // unlock main flash, write 0xAA to addess 0xX555 *(FLASH_COM_XAAA) = 0x55; // unlock main flash, write 0x55 to addess 0xXAAA *(FLASH_COM_X555) = 0x80; // write 0x80 command to erase entire chip *(FLASH_COM_X555) = 0xAA; // continue unlock sequence *(FLASH_COM_XAAA) = 0x55; // continue unlock sequence *(FLASH_COM_X000) = 0x30; // write 0x30 command to erase 1 sector should I use the PAGE register differently? or should I use a different type now for the address instead of ''xdata''? Thank you.2011-05-17 03:05 AM
Hi,
I corrected this problem by setting the PSDSoft to ''Program and Data Space'' for main flash programing of a page is possible and storing code on other pages. my question is if there is a way to define a pointer to a specific page, so by accessing the pointer the page register will change automatcaly? I tried enabling in uVision2 the far type, but all the banking configuration has reseted, and the extended linker has errors. I don't think there is another way, maybe pdata. [ This message was edited by: std on 29-12-2004 13:05 ]2011-05-17 03:05 AM
Hey,
I was searching ST's site for a multi-paging demo and I couldn't find one for the dk3200. BUT I did find one for the dk3300, which is almost identical to the 3200. This demo provides seemless page-to-page function calls and more. dk3200 & dk3300 demo's are here: http://www.st.com/stonline/products/families/memories/psm/soft_c2.htm The banking demo is called: dk33dsn4 (i think). This is pretty much a hello world app, but it uses all 8 pages. Simply make the necessary mods to run this on the dk3200 instead. Hope I could help.2011-05-17 03:05 AM
HCONST can be mapped to the banked area.
but HDATA ca not!! so how can I write to main flash without specifying the page value first????