cancel
Showing results for 
Search instead for 
Did you mean: 

JTAG flash software

marcus23
Associate II
Posted on December 13, 2004 at 04:10

JTAG flash software

3 REPLIES 3
marcus23
Associate II
Posted on December 08, 2004 at 03:55

Hi all,

is there any software to program the internal and the external flash of the STR710 without using the RealView Developer Kit? I need a software for end-of-line programming, so the RVDK is not the right software, as I need a batch or script configurable tool for flashing. Maybe there actually is some flash software that works with a wiggler-compatible interface?

thanks for your help,

Marcus

omar
Associate II
Posted on December 08, 2004 at 07:04

Hello,

for programming tool, there's two offers from 3rd parties:

1.Memtool from PLS (www.pls-mc.com) standalone software interface that can be integrated in automatic environment. y

2. J-flasher from Segger (www.segger.com) (standalone software interface used with j-link )

Regards

marcus23
Associate II
Posted on December 13, 2004 at 04:10

That sounds good,

thank you