2010-07-20 02:07 PM
Hello all,
I am using the IAR Embedded workbench and I'm noticing that when I am in debug mode and press 'Reset', the ISPR registers do not get reset (noticing from memory readout). This causes the interrupt service routing to get triggered immediatly after I configure them. This does not happen when I cold-boot or enter debug mode the first time. Have any others run into this? Is there a configuration option that would fix this or do I need to clear out the memory manually on boot?
Thanks,
Andrew Klofas
#debug #iar #interrupt #ispr