cancel
Showing results for 
Search instead for 
Did you mean: 

INDART for ST72C334

cecovic
Associate
Posted on June 27, 2003 at 06:22

INDART for ST72C334

1 REPLY 1
shreya
Associate II
Posted on June 27, 2003 at 02:46

Hello,

The error can mean two things

1) Incorrect application : The s19/elf/abs file which was downloaded is a different one, probably from an earlier build. Delete all the .o and .s19 files and rebuild.

2) Incorrect downloading : There is a problem with downloading the application which would appear as bad synchronization between source code and disassembly window. In that case, go to output window, click on 'Console' tab, select 'Verbose' and give command :

open-application ''''

I hope this helps.