2008-06-02 07:49 AM
In USB New FWLib ST Micro needs a new Function USB_DeInit()
2011-05-17 12:53 AM
I was having a LOT of problems with an Unstable USB when coming out of a HW Reset, not a Power Up Reset
This solved a lot of problems Don't forget to be in disabled IRQs This and other like it needs to be RIGHT after main or be done in Assembly and placed in 91x_init.s There looks like a LOT needs to be in 91x_init.s See Timer 0 - 3 problems that are now solved by doing a TIM_DeInit(), this needs to be in 91x_init.s // ************************************************ // A system reset does not reset the USB registers. // ************************************************ void USB_DeInit(void) { _SetCNTR(0x0003); _SetISTR(0x0000); _SetDADDR(0x0000); _SetBTABLE(0x0000); } :-(