cancel
Showing results for 
Search instead for 
Did you mean: 

In circuit bootloader via RS232 or USB ?

jas
Associate II
Posted on February 08, 2007 at 20:23

In circuit bootloader via RS232 or USB ?

33 REPLIES 33
shangdawei1
Associate II
Posted on May 17, 2011 at 09:30

any news about the source files for the DFU ?

twinknight
Associate II
Posted on May 17, 2011 at 09:30

use STR750F

shangdawei1
Associate II
Posted on May 17, 2011 at 09:30

Any news on the boot loader ?

vaclav2
Associate II
Posted on May 17, 2011 at 09:30

Hi

I read pdf file about UART bootloader and I have one question. Is the start adress of bank 0 after remaping by CAPS 0x80000 or 0x8000? Bank1 has only 32kB adress space.

Best regards

Vendelin

vaclav2
Associate II
Posted on May 17, 2011 at 09:30

Hi

I read pdf file about UART bootloader and I have one question. Is the start adress of bank 0 after remaping by CAPS 0x80000 or 0x8000? Bank1 has only 32kB adress space.

Best regards

Vendelin

najoua
Associate II
Posted on May 17, 2011 at 09:30

Hello Vendelin,

Bank0 is remapped to address 0x80000 using CAPS and Bank1 size is 32Kbytes as you said.

Regards,

Najoua.

[ This message was edited by: Najoua on 07-02-2007 09:57 ]

ron2
Associate II
Posted on May 17, 2011 at 09:30

I was just reading an article in embedded-Developer.com. Here is the link.

http://www.embedded-developer.com/tools/470/STMicroelectronics/um0290.htm

It says that the USB Boot loader called a DFU. What does DFU stand for?

Is available in the USB developer kit.

I haven't checked it out yet but it is something I need for my project.

:D

sr_shinde2
Associate II
Posted on May 17, 2011 at 09:30

Hi All,

Will This bootloader work for STR912FAW46 ?

Regards

Sai

davidwilson9
Associate
Posted on June 28, 2011 at 09:44

Where is the link to download?

Posted on June 28, 2011 at 20:47

Where is the link to download?

AWOL

The thread is from 2006/2007, a prior incarnation of the forum, and user database. The current forum had a meltdown in mid May 2011. Attachments have not survived these processes, ST might be able to dig them out of the archives, but that's not certain. You may want to check if the material is mirrored other places on the net, or that the posters are active on other forums.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..