2006-03-21 10:39 PM
idesc copy from RAM to ROM using fctcpy
2006-03-08 12:02 AM
Hi,
I want to locate the idesc generated by the linker in the ROM to RAM using the _fctcpy() function call from an assembly file. Kindly let me know whether this is possible. ;)2006-03-08 03:39 AM
2006-03-08 04:11 PM
Hi Luca,
Yup. The compiler used is Cosmic and it is for the ST7 micro ST7FL35. My project is right now using the crtsx.s file provided by the cosmic, and i could see from the file that the idesc generated by the linker in the ROM is copied to the RAM. but i would like to modify this asm file by using the _fctcpy() command. is it possible to do so ? are there any examples for this? Regards, Suganya2006-03-08 07:47 PM
Hi,
you are mixing two different things here: the _idesc_ symbol is used for automatic data initialization, whereas _fctcpy() is used to copy and execute code from RAM. So the answer is no; what you want to do is not possible. Still, I'm curious to understand WHY you would want to do anything like that: if you need automatic data initialization, crstx.s in the most efficent way to do it, and if you don't need it, you can use ctrs.s and save some bytes. Regards, Luca (Cosmic)2006-03-09 08:23 PM
Hi luca,
Thanks! Now i am going ahead with the crstx.s, and i have a clarification in it. My MAP file tells me the bss region as, start 00000104 end 00000108 length 4 segment bss But when the following statement in the crstx.s file is executed it gets the start address of the bss value as 0108 which is the end address and hence it does not initialize the bss region. ld x,#low(__sbss) ; address LSB in X X - register gets loaded with 08 here, i am expecting 04. Please can i know what could be going wrong ? Regards, Suganya2006-03-10 01:42 AM
that's strange; I tried a similar project here and it seems to work ok.
I sugget you do the following, possibly with a simulator: - load your project - fill the memory with a recognizable value (ex: 0xA5) - put a breakpoint on main() - run - check the memory, where you believe your bss is If it's 0, then the startup file somehow cleaned it; execute the startup step by step to undersand what it does exactly If it's not zero (it will likely be 0xA5), than the startup did not initialize it correctly; post your project here so that I can see what's wrong. Regards, Luca2006-03-13 06:47 PM
I am not able to see my bss cleared still. In the map file i am able to see that my bss region is from 0x0104 to 0x0108 and I carried out the steps stated by you, but this region was not cleared. I have attached my project.
Kindly let me know what is the problem. ________________ Attachments : tutorial_cosmic.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0AO&d=%2Fa%2F0X0000000bVq%2FIHmMTFAyQhh4hQDP9bwcjJuBUw1EpmMsHVIHT8lRuPk&asPdf=false2006-03-13 08:54 PM
the attached application does not build.
Modifying one line of the linker file from +seg .share -a .bss -is # simulated stack to +seg .share -a .ubsct -is # simulated stack I'm able to build and the initialization of the bss is ok (starts from 104) Make sure you are using the objects that you are compiling (maybe try to rebuild this project on a new machine), and try the init with a simulator. Regards, Luca [ This message was edited by: _luca on 14-03-2006 10:27 ]2006-03-13 11:58 PM
Luca,
I am not getting that error, i am still working on it. Between correct me if i am wrong, The model which i have choosen is modmm, in that case the stack is to be located in the long range. then in that case following bss region should not be of problem right? and can we locate after the .ubsct region, would'nt that be short range of the stack? Regards, Suganya