cancel
Showing results for 
Search instead for 
Did you mean: 

IAP

shermantec
Associate II
Posted on July 21, 2003 at 19:07

IAP

2 REPLIES 2
shermantec
Associate II
Posted on May 17, 2011 at 11:55

Hello

My boot is from the Second Flash and i want to load another program to the Primary Flash from the RS232 - for this i need to use the IAP feature but i don't find any information about this for the uPSD .

The only information available is for PSD and this is not the same .

Pl's advice support .

Latino from Israel
joseph2399
Associate II
Posted on May 17, 2011 at 11:55

Currently we do not have IAP code written for the uPSD family. You will have to develop your own IAP code. We already have a few customers got their IAP code working. They all used the IAP code written for our DK900 eval board as a starting point and modified it to work with the uPSD. AS you know, DK900 eval board uses a standard 8032 MCU and a similar kind PSD as the one used on the uPSD.