2007-04-18 01:54 AM
2011-05-17 02:51 AM
Hi to all,
I make my first steps with the upsd 3334 and I'm trying to switch between 2 programms. One in the main flash and one in the scondary flash. After pressing a button on the DK 3300 I change the VM Register to say that main flash is program space and secondary flash is data space and the other way around. After writing in the VM Register the upsd stops working.Can somebody help me ? I would be pleased also much about an example with IAP. Finally I want load a program of 64 KB over a serial interface into the main flash. regards bombenhorst :o