2007-11-09 02:33 AM
IAP driver with EWARM and J-Link
2011-05-17 12:47 AM
Hello arno,
The IAP driver should be located in Bank1 after being hardware remapped at address 0x00 using CAPS tool. So, did you remap Bank0 and Bank1 to 0x80000 and 0x00 respectively using CAPS tool? Regards, Najoua.2011-05-17 12:47 AM
I have compiled the IAP code with the EWARM 4.41 and try to load it with the J-Link. It seem's that the code is loaded in 0x20000 and the program don't start.
Please, what should i do ?