2007-05-30 03:50 AM
2011-05-17 12:43 AM
Hi,
A STR912 device is connected via I2C to a pic controller. The STR912 asks 4 bytes over I2C. When I use a non interrupt driven communication, it works OK. When I use interrupt driven communication, after receiving the first 4 bytes, I generate a stop condition. After doing this, I get continuesly an interrupt but no Eventflag is set. How is this possible ? If somebody has some idea, plz help me before I become crazy... :-Y Luc