2024-03-19 06:19 AM - last edited on 2024-03-19 10:22 AM by Peter BENSCH
Hey there , how can I find info to conect my STM32 with higher voltage devices , for digital inputs and outputs I have 24vcc and analogic inputs and outputs -10 to 10v, I want to conect they safely to not burn my chip.
Solved! Go to Solution.
2024-03-19 12:48 PM
I have to hand it to you: you give a lot of details about your project and we have now a complete overview of all boundary conditions (irony = off).
You will need matching circuits in any case:
Hope that helps?
Regards
/Peter
2024-03-19 10:40 AM
Welcome @Chris8, to the community!
As long as it is not clear which STM32 you have in mind, I have moved the thread to Other Hardware, as you need some kind of signal conditioning in the broadest sense.
It is not entirely clear what exactly you want to do, among other things there are no details of which parameters are required in detail:
For the inputs, additional details such as the required pulse strength for the input voltages or input impedances are important:
Other important details for the outputs are e.g.:
As you can see, there are more open questions than you have expressed wishes. Can you go into more detail?
Regards
/Peter
2024-03-19 11:22 AM
I buy a STM32F411 and on digital inputs I ll conect +24v sensors , on analogic input -10 to 10v sensor , on digital outputs ll go to driver +24v digital input , and analogic output I want deliver -10 +10v for control a motor driver ( I want this signal analogic not pwm wave) frequncy of project is less than 10khz
2024-03-19 11:26 AM
2024-03-19 11:42 AM
on servo driver is 10k ohms for analog
4.7k ohms digital
Im using NPN 24v festo hall sensors
2024-03-19 12:48 PM
I have to hand it to you: you give a lot of details about your project and we have now a complete overview of all boundary conditions (irony = off).
You will need matching circuits in any case:
Hope that helps?
Regards
/Peter