2018-02-09 12:06 PM
Board boot ok
WiFi connect Pc or Tablat ok (192.168.0.2)ping 192.168.0.1 ok
https://community.st.com/external-link.jspa?url=http%3A%2F%2F192.168.0.1%2Fcommand.shtml
load ok
click to button (Send the command) G-conde command line M115 --> no action and no Platform respond
or
https://community.st.com/external-link.jspa?url=http%3A%2F%2F192.168.0.1%2Ffilemgt.shtml
load ok
G code file monagmentclick to button (Get G codes file list) --> no action and no Platform respondor
3D printer configuration fileclick to button (Get config) --> no action and no Platform respond--> nothing happens
--> wifi connection error
ping 192.168.0.1 --> Destination Host Unreachable--- I do
sw4stm32_linux_64bits-v2.4 - install
Firmware download en.stsw3dp001.zip
Project import in 'System Workbench for STM32'
Build Project ok
Marlin.bin --> Board flash okDebug Project no problems visible - no errorBoard boot ok
click to button--> nothing happens
--> wifi connection errorCan you help me, what can I do.
Is the board faulty?
#wifi #stsw-3dp001 #3d-printer-board2018-02-12 02:45 AM
Hi !
First your post appears as 'assumed answered', why ?
On topic, I have the same board, and if I'm correct, the web server is handled entirely by the wifi chip, and it will communicate only what is needed to the F401, which handles all the hardware side. Also I think that you need an SD card with some specific files on it (this is a marlin stuff). Again I am not really sure...
I must say that the support for this board is not top notch, at least on this forum. Maybe if you ask directly ST you can have a better answer...
2018-06-07 03:16 AM
i got totally the same problem with you ! did you solved it ? i cant change the name ssid and the password of wifi also. so i think problem is communication from wifi module and st chip. but still cant fix yet. if you have the solution. please put it here or send me an email at :
mailto:chimchichclick@gmail.com
! thanks !2018-06-07 10:47 PM
i using IAR ide and problem is solved. so, i dont know where is problem with SW4STM32 IDE