2007-05-02 03:31 AM
Further question on the IAP application note
2007-04-30 05:37 AM
Hi,
I had problem last week to compile the AN2078 IAP. Now it compile ok but I have trouble to adapt it to my application/hardware. Here's my questions 1) In the AN2078 documentation, on page 3 there is noted that for the STR71x the code should take 7.2KByte. Compiled in release mode, my AXF file is 32.6 Kbytes. Is this normal ? 2) When I want to program my application from the IAP, should I use the AXF of my application program (and juste modify the load region in the scatter file?) thanks in advance2007-04-30 10:32 PM
maybe some information about my case could help someone in helping me :-]
So currently, the IAP is booting ok on my hardware, I see the menu in hyperterminal. It seem that the flashing is ok, I can send file like explained in the documentation, but after the transfer there is some garbage in hyperterminal (after the downlad) :Code:
Programming Completed Successfully!
-------------------------------- Name: debug.axf Size: 102724 B================ DownloadJµ…â€¢To the STR71x Internal Flash ---------- 1 Execute The New Program ------------------------------ 2 After that, I can't run my program. The strange thing is that if I shutdown and restart my device, the IAP don't run anymore. So I suspect that I have messed up something with my modifications to make it run on my hardware. As I said in my first post, the IAP axf file is about 32kb, but when I program it with the JTAG, it show that he program only the two first sector (0&1) of the bank 0. So I have modified the IAP to flash my program on the beginning of the third sector of bank 0 (0x40004000). I have modified my application scatterfile like this :Code:
USER_MODE 0x40004000 0x30000 { FLASH 0x40004000 { 71x_init.o (Init, +First) * (+RO) } RAM 0x00000000 { 71x_vect.o (Vect, +First) * (+RW) * (+ZI) } } And modified 71x_init.s to do ram remapping. If something writen above sound for you like an heresy, please put me on the right way ;-)2007-05-01 10:16 PM
Hello tumnao,
In the IAP driver provided by ST, the user application will be loaded beginning from Bank0 sector1 base address. Before loading the application, a check of its size is done in the routine FLASH_SectorMask() in common.c source file (this routine is called in ymodem.c in Ymodem_Receive() routine): if user_application size < 8kbytes --> sector1 will be erased if user_application size < 16kbytes --> sectors 1 and 2 will be erased if user application size < 24kbytes --> sectors 1, 2 and 3 will be erased etc... In your case, the IAP is located in Sectors 0&1 so sector1 shouldn't be erased. So, the routine FLASH_SectorMask() in common.c source file should be updated as follow: u32 FLASH_SectorMask(vu32 Size) { if (Size <= 0x2000) return 0x4 // instead of return 0x2; if (Size <= 0x4000) return 0xC // instead of return 0x6; if (Size <= 0x6000) return 0x1C // instead of return 0xE; if (Size <= 0xE000) return 0x3C // instead of return 0x1E; if (Size <= 0x1E000) return 0x7C // instead of return 0x3E; if (Size <= 0x2E000) return 0xFC // instead return 0x7E; //if (Size <= 0x3E000) this case is no longer valid because the user application size shouldn't exceed 256 - 16kbytes = 240kbytes. //return 0xFE; return 0; } You said ''The strange thing is that if I shutdown and restart my device, the IAP don't run anymore'' --> the IAP driver can be re-executed under a specific condition at RESET. This condition is a Low level on P1.8 pin. For more details, please refer to AN2078, the section 2.2 Triggering execution of the IAP driver, page 5. Hope this helps you, Best regards, Najoua.2007-05-02 01:47 AM
Many thanks Najoua, you where right.
This explain me why my IAP didn't work after a programming, he was erasing himself... And since my last post I also found answer to some of my question by activating the size report in the linker message option... My program is smaller that i thinked :-) And I also found the fromelf tool. By reading the RVDK linker guide I suspect that I need to convert my AXF to bin with it. Still no working IAP, but closer than never :-]2007-05-02 02:23 AM
2007-05-02 03:31 AM
Yeah, I didn't forget to do that, and after reading the fromelf doc, IAP is working ! :-]
My last problem is about interruption so I must have messed something up in the ram remapping process. But this is a big step for me, as this is my first embedded project I have a lot to learn and each new working functionnality make me really happy. Thanks to all the helpfull people posting in this forum ;-)