cancel
Showing results for 
Search instead for 
Did you mean: 

From Debug to Release - problems with INTVEC.

johnsim
Associate II
Posted on September 19, 2005 at 09:53

From Debug to Release - problems with INTVEC.

2 REPLIES 2
johnsim
Associate II
Posted on September 16, 2005 at 14:03

Hi,

changing from Debug to Release mode in IAR Embedded Workbench, using a the LED_DIMMER example as a starting point, I'm getting the following error when linking:

Error[e16]: Segment INTVEC (size: 0x428 align: 0x2) is too long for segment definition. At least 0x3e8 more bytes needed. The problem occurred while

processing the segment placement command ''-Z(CODE)INTVEC=00-3F'', where at the moment of placement the available memory ranges were

''CODE:0-3f''

Reserved ranges relevant to this placement:

0-3f INTVEC

Basic project is the same, but I've added in XTI and EIC files for my project. I've also commented out the in 71x_conf.h to change the library to release mode from debug.

Any suggestions what this is and how to fix it? I can only find one reference to INTVEC in Inkarm.xcl

Thanks,

John.

johnsim
Associate II
Posted on September 19, 2005 at 09:53

Thanks ibtiss, that did the trick!

John.