2008-11-14 12:40 AM
2006-09-08 01:36 AM
Hello,
there are the good applications ''DfuSeDemo'' and ''Dfu File Manager'' (and all works fine) I see the *.hex file is converted to *.dfu file, which is (except the first ~100bytes) the same as the *.sim file. Now are on work to programm our own download software. Is there any documentation available ( e.g. for the application ''DfuSeDemo''). My question is: what is the start address (first byte) from the download file (*.dfu). What is the requirement for a correct download? Thanks, Heribert2006-09-10 10:48 PM
Hello,
so i see there is to use the *.bin file for download.2008-11-14 12:40 AM
Hi ! This DfUse application comes with a button to Enter DFU mode/ HID detach and leave DFU mode. Does anyone have a example of a HID firmware with DFU support, I mean a HID/DFU compliant device?