2004-05-17 01:59 PM
2011-05-17 03:00 AM
Hi,
I got DK3300 eval kit for µPSD33xx. I have some problems to let run the board : I tested Flashlink with µPSD Softexpress to program Flash on board : all is fine. I want to test the part in debug mode so I place the jumper in right position. When I try to use Link from Keil, this tool is seen by microvision2 debugger as USB device. Although, when I try to start debug, an error comes : ''JTAG device chain error'' Is someone can help me ?2011-05-17 03:00 AM
Please send an e-mail request for an upgrade of the DK3300 kit that includes rev C silicon. The e-mail address is
mailto:apps.psd@st.com
. Please include the following information: Name Company Name Phone Number Ship to Address Location (City, State, Country) uPSD part number of device being used (3334, 3354, etc.) Application Projected annual volume (units) Regards, uPSD Applications Engineering [ This message was edited by: uPSD on 18-05-2004 02:32 ]