cancel
Showing results for 
Search instead for 
Did you mean: 

Debug information with JTAG Interface?

heribert
Associate II
Posted on September 05, 2006 at 11:50

Debug information with JTAG Interface?

2 REPLIES 2
heribert
Associate II
Posted on September 04, 2006 at 07:36

Hello,

i also have trouble to run the ''B-Programm'' after the IAP initialisation.

My question: is it possible to view the initialisation and jump to B-MAIN via the JTAG-Interface in any way?

(I see in program A the jump to B) Is it possible to view the B-program initialisation alone?

Thanks for help.

I use IAR and J-Link.

heribert
Associate II
Posted on September 05, 2006 at 11:50

Hello again,

the IAP Driver (--> Bootloder or B-Program) works fine with connected JTAG Interface and debug mode. I wrote the bootloader with start-and end-address, B-Programm is still in the flash. In standard mode (with or without)connected JTAG Interface it doesn't work. With connected JTAG Interface, after a reconnect the USB plug on the JTAG Interface it runs.

Only programming B-Programm, so all works.

Does anyone have an idea, what is wrong?

Thanks Heribert