2018-04-11 06:37 PM
Dear helper:
I got a question about the Low side switch IC L98
The conmunication mode of this IC is SPI. It is unbelievable that the SCK high time is specified as 160ns based on the datasheet. The time can't exceed 160ns or is less than 160ns, which is riduculous. Generally, the SPI clock frequency has a maximum value, not as mentioned in the datasheet.I want to know if there is an error in the datasheeet?