2003-12-10 12:13 AM
Converter utility - ''*.abs'' to intel-hex
2003-12-08 11:57 PM
hello forum,
I'd like to convert my ''project.abs'' output (metrowerks - 72F521) to intel-hex or motorola-s format for burn my target application with 'DataBlaze programmer'. please attache this utility file or point me to download it from internet site. thanks atz2003-12-09 03:20 AM
you can either use Burner utility included with metrowerks or use -B option on the linker command line.
Regards sjo2003-12-09 04:13 AM
hello sjo
thanks for your help. the output file of -B option creates a 'project.sx'. (it seems as S-rec) I burn it with the 'DataBlaze' and after reset in my demo board it works. but the moment I plug off the emulator (indart-stx) ICP connecter, re-power the demo board and do reset it dosen't work. How do I burn the ST72F521 thus it will work stand-alone (with no development tools) ? tanks. atz2003-12-10 12:13 AM
Check your options/oscillator are configured correctly.
Regards sjo