2005-07-19 02:51 AM
Application AN1763 ( batery supllier)
2011-05-17 03:07 AM
I have a problem in my design with one uPSD3312, and sometimes the XDATA value changes, maybe the battery supplier is less than 2 volts that the manufacture ask for keep the dates ( I don´t think so ). Someone can tell me why in the application note 1763 in the schemaquic appear one coil of 100 uH and one capacitor of 104p. If I put this in my design I will eliminate problems with eventual noise in the battery supplier or not. Thanks.