2004-09-13 04:54 PM
About the Enhanced Interrupt Controller
2004-09-09 11:01 PM
In the AN1776.PDF, the user program run in the SYS mode. when the an interrupt occurs, system jump to IRQHandler.
Why is the mode SYS mode and not USR mode? If the mode is USR mode, the routine is same.2004-09-13 04:54 PM
Thanks, I see, but I have another question:
why to change IRQ mode to SYS mode, why does program not deal with the interrupt task in IRQ mode?