2017-06-20 04:43 AM
Hello All,
I am working on SPC560B54L5 board using SPC5studio version 5.2.3.
I am trying to generate the clock output using the XOSC frequency. I enabled the corresponding GPIO (PA[0] for CLKOUT) by selecting the appropriate alternate function. In main function after doing the componentsinit(), initialization of spc_clock_init(); is done for output clock selection. Later I am enabling the output clock by writing to the CGM.OC_EN register.
But still I am unable to find the clock output on the corresponding pin. (PA[0]-> X1(19)).
I am attaching my test application for reference, kindly check and provide your valuable suggestion towards the issue.
Thanks in Advance,
With Regards,
R.Santhamurthy
Solved! Go to Solution.
2017-06-20 06:13 AM
Hello ,
You can see in your discovery board the differents lines X1,X2,X3,X4.
cf Document B_DISCOVERY.
the pin nearest X1 is 1 and so on ...(2,3 until 19)
Best Regards
Erwan
________________ Attachments : DM00094991_B_DISCOVERY.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyAW&d=%2Fa%2F0X0000000bA4%2FXKw6NjiytMc_DkLx7Tl1uPo999KwecNm8RW6fyKJeHk&asPdf=false2017-06-20 06:13 AM
Hello ,
You can see in your discovery board the differents lines X1,X2,X3,X4.
cf Document B_DISCOVERY.
the pin nearest X1 is 1 and so on ...(2,3 until 19)
Best Regards
Erwan
________________ Attachments : DM00094991_B_DISCOVERY.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyAW&d=%2Fa%2F0X0000000bA4%2FXKw6NjiytMc_DkLx7Tl1uPo999KwecNm8RW6fyKJeHk&asPdf=false2017-06-20 08:51 AM
Hi Erwan,
Thanks for your Reply.
I am clear with the pin configuration and the pin numbers in my discovery board.
With my previous post in this chain, I am trying to convey that, If I try to check the frequency of the output clock at X1-19 (CLKOUT pin) using oscilloscope, I am not getting the clock output. As per the configuration in the application attached with the post, I should get 16MHz clock frequency output at X1-19 in my board. But I am failing to get the result.
Kindly check the attached test application and support in getting the problem resolved.
Thanks in Advance,
With Regards,
R.Santhamurthy