cancel
Showing results for 
Search instead for 
Did you mean: 

manual issue SPC570s?

Posted on October 12, 2017 at 08:49

Hi,

in the memory map of the reference manual of SPC570s the SARADC_B has an address of 0xFFE3_C000.

This seems to be right, because it works fine with that address.

But 3 lines down under this address is marked as Reserved.

Logical the line of SARADC_B would be 0xFFE0_4000.

0690X00000608WfQAI.png
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 REPLY 1
Erwan YVIN
ST Employee
Posted on October 12, 2017 at 09:18

Hello Michael ,

2 issues is noticed on the last revision of RM table 12 (Rev6 RM0349)

I am forwarding the point in technical writer team.

  • PCTL is not correct it should be 112 or 113 for SAR_ADC_12BIT_B0
  • reserved address is not correct
0690X00000608aBQAQ.png0690X00000608UaQAI.png

           Best regards

                    Erwan