2017-09-21 9:51 PM
hi everyone ,
I am using SPC560B discovery board , I am new to spc5 studio ,could someone help me how to configure the WAKEUP PINS to wakeup the MCU from STOP mode . My requirement is the MCU should identify the wakeup happens by which pin exactly kindly someone help on this issue,My application is to wakeup the MCU from GSM RI interrupt pin and also when the MCU is running mode it should get interrupt from RI pin.2017-09-25 2:13 AM
Hello Avinash Puli ,
There are some examples
how to use the WKUP Interrupts in this following application (Cf Application Wizard)
SPC560Dxx OS-Less WKPU LPM Test Application for Discovery
Best regards
Erwan