missing-QuestionPost

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CRC calculation with DMA

Posted on October 06, 2017 at 11:31Hi guys,i tryed to use the CRC Modul with DMA Access but it doesn't work.My first step is to configure the DMA Channel.DMA.TCD[3].SSIZE = 2 /** 4 Bytes **/DMA.TCD[3].DSIZE = 4DMA.TCD[3].SOFF = 4DMA.TCD[3].DOFF = 0D...

Synchronous rectifier using SPC570S-DISP board

Posted on October 23, 2017 at 07:16Hi ST experts!I have worked on phase shift full-bridge converter projects. Recently, I get a trouble with synchronous rectifier PWM. The PWM duty, frequency, and deadtime parts work well, but they can't not shift p...

Tran Hung by Associate II
  • 1054 Views
  • 6 replies
  • 0 kudos

manual issue SPC570s?

Posted on October 12, 2017 at 08:49Hi,in the memory map of the reference manual of SPC570s the SARADC_B has an address of 0xFFE3_C000.This seems to be right, because it works fine with that address.But 3 lines down under this address is marked as Re...

0690X00000608WfQAI.png

Interrupt and wakeup pins configuration SPC560B

Posted on September 22, 2017 at 06:51hi everyone ,I am using SPC560B discovery board , I am new to spc5 studio ,could someone help me  how to configure the WAKEUP PINS  to wakeup the MCU from STOP mode . My requirement is the MCU should identify the...

Resolved! FlexRay SPC56EL70L5

Posted on August 08, 2017 at 08:29Hello community,I am asking myself if there is actually anyone running FlexRay on the SPC56EL70L5 Board?I am currently stuck in the wakeup process (I think that is where I am stuck), because the wakeup pattern does ...

How to enable interrupt without OSAL and HAL component

Posted on August 10, 2017 at 10:54Hello!I made new project only using SPC560Bxx Platform Component in SPC5 studio.When I add OSAL component, Interrupt does work well.At present, I am trying to enable interrupt without OSAL and any HAL component. But...

Hank Im by Associate II
  • 964 Views
  • 3 replies
  • 0 kudos

Power supply of SPC560P34L1

Posted on August 09, 2017 at 12:46Please can anyone help me, i'm working with SPC560P34L1, i will use the UART interface, CANflex module and  flexPWM module(one pwm output), i need to know how much current can this MCU consume, in orther to provide ...

AC MR by Associate
  • 529 Views
  • 2 replies
  • 0 kudos

Flash library

Posted on August 03, 2017 at 13:07Hello,I’m developing SPC58xC(SPC584B70E5) Flash driver now, I want to know how to get the C55  Flash library?Thanks a lot.BR,Sijia