2019-01-07 05:47 AM
It's possible programming the SPBTLE-1S using UART pins or just in SPI pins?
If possible, how can I made it?
If it's just using SPI pins, how can I made it?
But if any options I said it's impossible, what's the best way to programming the SPBTLE-1s and how can I use?
I have tried using the STM32L152RE and the STM32L072RBT6
2019-02-22 03:51 AM
Hello friend, have you solved the question?
2019-02-25 06:50 AM
No. But I trying to use the X-NUCLEO-IDB05A1 with STM32L152RE but without success yet